3/5
  • Pages

—

A rock-solid commitment to sustainability

Raw material preparation, milling and kiln operations can be significant producers of sulfur dioxide. Increased regulations means that producers are on the hook for major fines for every emissions violation. In order to meet their operating targets and reduce the risk of violations, CEMEX worked with ABB to reduce deviations around its daily SO2 emission targets for its Rüdersdorf plant.

> Discover ABB Ability Expert Optimizer

—

A rock-solid commitment to sustainability

Raw material preparation, milling and kiln operations can be significant producers of sulfur dioxide. Increased regulations means that producers are on the hook for major fines for every emissions violation. In order to meet their operating targets and reduce the risk of violations, CEMEX worked with ABB to reduce deviations around its daily SO2 emission targets for its Rüdersdorf plant.

> Discover ABB Ability Expert Optimizer

ABB Ability Expert Optimizer is an advanced process control application that uses model predictive control, fuzzy logic and neural networks to optimize cement plant operations. CEMEX uses ABB Ability Expert Optimizer at its Rüdersdorf plant to minimize the effects of variability in its feed and fuel sources, making it simple to establish the advanced process control techniques required to reduce SO2 emission variability.

CEMEX uses ABB Ability Expert Optimizer to automatically optimize the short-term exhaust SO2 target based on the current daily average. Two optimization modes allow the operator to select either normal or aggressive optimization based on whether to target the daily average below the limit at the end of the day or within the next 30 minutes. ABB Ability Expert Optimizer automatically adjusts the multiple feeder points of lime hydrate to ensure the SO2 and HCL targets are stringently met.

CEMEX uses ABB Ability Expert Optimizer to automatically optimize the short-term exhaust SO2 target based on the current daily average. Two optimization modes allow the operator to select either normal or aggressive optimization based on whether to target the daily average below the limit at the end of the day or within the next 30 minutes. ABB Ability Expert Optimizer automatically adjusts the multiple feeder points of lime hydrate to ensure the SO2 and HCL targets are stringently met.

ABB Ability empowers insights for safer, smarter operations that maximize resource efficiency and contribute to a low-carbon future.

LEARN MORE